Other Parts Discussed in Thread: UCD7242, TMS320C6678
Dear engineer of TI, I am in the process of debugging the UCD9222 and UCD7242 power module. I used the Fusion Digital Power Designer v1.8.230 and use the Firmware Download Tool to download ".x0 " program and data file, run the GUI ONLINE mode, the monitor interface shows that the input voltage and temperature, but there is no output voltage and output current, the Status Registers show a yellow warning" output off" and "powergood#", other items show OK. You can see the following picture.
At this moment, the monitor data is still in sync, although there is no output voltage and current, but you can see the green plot line extends to the right near zero. When I pull up the control line to high level, all of the monitor data are out of sync and you can see all the green plot lines stop moving to the right, just like I shut off the power. The Status Registers still show a yellow warning "output off "and" powergood# ", other items show OK. You can see the following picture.
I try to clear the configuration and use the Firmware Download Tool to download ". x0 " program and data files again, found UCD9222 seems locked, can not find the device, you can see the phenomenon in following picture:
The ".x0 " program and data files was export by the GUI and using project file “TMDXEVM6678L_UCD9222_16May11_ver5.xml” which was found in TI's official TMS320C6678 EVM board “TMDXEVM6678L EVM” program files, and my PCB used nearly same design with TMDXEVM6678L EVM board, you can see the schematic in following pictures:
In addition, I also tried to used TMDXEVM6678L EVM board to run GUI online mode. At the beginning, the Status Registers also show a yellow warning" output off" and "powergood#" and other items show OK. But when I pull up the control line to high level, the output voltage and current appeared, and the monitor data is still in sync. You can see the following picture:
Now I want to consult the TI engineer's expert on digital power: 1. why the UCD9222 monitor data ware out of sync in my PCB when I pull up the control line to high level, but TMDXEVM6678L EVM board can’t be. 2. What cause the UCD9222 locked and can’t be recognized by GUI. How to unlocked it without replacing the IC. Thank you very much!