Hi,
My customer is considering to use VP voltage for other devices. They think that it can be used within the power rating of NPN transistor. Can you recommend it?
Best Regards,
Satoshi / Japan Disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is considering to use VP voltage for other devices. They think that it can be used within the power rating of NPN transistor. Can you recommend it?
Best Regards,
Satoshi / Japan Disty
Hi David,
Here is the additional information. Can you give your comment for these information?
Best Regards,
Satoshi
Satoshi,
Thank you for the clarification.
For this use, it should be okay to load VP within the power limits of the FET/resistor. I will try to put a small load on our EVM on Monday to see if anything weird happens with the dynamic load, but it should be okay.
My concern now will be thermal performance and the voltage drop across the TOP resistor. I just ask that things are sized appropriately. Last I knew, there is a small possibility that there is a 40mA transient at startup (a random event with a very small chance of happening). This can prevent the part from starting up in some cases, but sizing the TOP resistor for this transient will eliminate that concern as well.
Hi David,
I really appreciate for your support. I'm waiting for your evaluating result.
Regarding the voltage drop across the TOP resistor what you are concerning. First, please let me know which is TOP resistor in attached schematic that is referred from Fig.36 in datasheet. I guess that you mean R104 and R105 as TOP resistor, then do you mean that there is possibility of 40mA transient pass through these resistor at start up? It will be appreciated if you will explain this again for clarify my understanding.
Best Regards,
Satoshi
Hi Satoshi,
I haven't had the opportunity to look at the switching load, but i think it will be okay. I will still look at it and reply if i get the chance today.
You are correct, i meant R104 and R105. I apologize for the misunderstanding.
Upon POR, there is a small probability that the device will pull 40mA during its start up, This spike should be very brief i believe, so if the resistor values are such that the voltage drop does not put the regulator in dropout it will be okay.
For example, say R104 + R105 = 1000 Ohms, and this event occurs. Then for a very brief instance, there will be 40V across these resistors. If the module voltage is low enough, it may not leave enough headroom for the VP regulator to work, causing the IC to lock up.
As long as the resistor values are chosen with this in mind, it should be okay.