This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138HSFBEVM-029: UCD3138HSFBEVM-029 Load Current Sensing Inaccurate

Part Number: UCD3138HSFBEVM-029

Hello, I did experiment with the UCD3138HSFBEVM-029. Among them, the GUI shows the output current value is the development board of the actual output current value of 0.7 times.For example, the actual load current is 2A and the GUI is shown as 1.4A ,why?