Other Parts Discussed in Thread: TPS92830-Q1
Dear Support team
Can I use TPS92638-Q1 without detecting fault at low voltage(Boost to battery)?
In my understanding, if the Fault pin is set to H, protection can be disabled at low voltage, but short / open protection is also desabled.
◆Spec
・Vin:10~16V
・Vout: 3LED×4string (Vf 3V)
・Iout:140mA/string
・Short/Open LED protection need.
Regards
Topmohiro Nagasawa