Hi,
I'm designing a LiFePO4 solar battery charger using the bq24650. As the title says, I need to achieve currents larger than 8A (max 10A). My current layout is a near exact replica of the EVM board layout with the difference that I have components only on one side of the PCB. My question is, with the EVM layout and using the same components, can the charger deliver 8A-10A charge current while keeping the mosfets at reasonable temperatures?
I already have a previous version of this charger which had the mosfet case temperature rise to 84C at a charge current of 5A. This previous layout had some bad layout techniques (Inductor pads extending underneath the inductor, mosfet to inductor track connected using parallel multi layer tracks, mosfet pads connected using thermal relieve etc... basically, all things that the datasheets lists on page 28 as Layout Guidlines were ignored). This made me think that there maybe an issue of loop stability in the charger too. I measured the mosfet drain/inductor voltage and there is no ringing. I also measured the rise/fall times and they are the same as seen in the datasheet. I did see some ringing in the inductor current though. I manually removed the extra copper from underneath the inductor and the current ringing decreased considerably but the rise in mosfet temperature remained.
Before sending the PCB to be manufactured, I would like to know if the design is even possible and if so, if there are other consideration to be taken. As a side note, I was thinking about using the BSC072N03LD mosfet instead of the Si7288DP due to it having a smaller RDSon value and a better FOM value too. Using the Ploss calculation given in the bq24650 datasheet, this mosfet should have roughly 1W dissipation at 10A as opposed to about 2W with the Si7288DP.
Again, is the design I'm making even possible or is it necessary to use single mosfets instead of a dual mosfet package (or even using two paralleled mosfets) and are there other considerations I need to take care about?
Thanks