Part Number: TPS65560EVM-165
I just purchased a TPS65560evm-165. A sweet circuit. And now for the questions;
1) I plan to position the circuit in an enclosure and operating it from a remote on/off switch on the enclosure, supplied by a 12VDC 3A wall wort. Can the charging and discharging push buttons be jumpered to allow for continuous operation ?
2) Removing jumpers JP1 and JP2 to isolate the flash tube, I would like to position a coil, one end connected to the C5 discharge post of JP1 and the other end of the coil to the J6 trigger terminal block, which will feed into the collector of the IGBT. The objective is to pulse the coil.