Part Number: TPS53319
Other Parts Discussed in Thread: TPS53355, TPS543C20, LM25119
I need to produce 3.3V 28A, from a 5V input.
I was looking at using 2x TPS53319 in parallel. The parallel option was preferred because in some variants just the 1 will be required.
The question is, can I use the TPS53319 in parallel without series diodes on the output? At 14A each chip, the diodes will be unacceptably inefficient.
If diodes are absolutely required, I will look at using ideal diodes. However they are too costly to use if unnecessary.
Thanks
Chris