hi
we are designing power section for an FPGA based system :application(Medical).
Q1: I need to convert 12v Dc voltage into both +150V DC and -150V DC ,the maximum current rating should be 0.5 A. Does any one suggest any IC based solution?
Q2: if no IC based solution , Whether I have to use Inverting Buck boost topology?or Flyback?
Q3: is any SMPS design already in this configuration by TI?
VIN=12V Vout1 =+150V Vout2=-150 Iout(max)=0.5A