This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24600: IC getting damaged

Part Number: BQ24600
Other Parts Discussed in Thread: BQ24610

Hello,

I am using bq24600 for charging Li-Ion battery pack of 4S-2P configuraion. However, I am unable to charge it when the pack is fully discharged. The actual problem where I stuck was IC getting damaged while connecting battery pack to the terminals. Following are the testing conditions.

1. Input supply voltage from regulated power supply is at 24 V.

2. Battery pack voltage is around 15V.

3. I started the circuit (same as in application note of bq24600) by giving 24 V from RPS and then I switched on MCB so that the battery pack is connected at the output terminals.

Here the problem comes, as soon as I switch on MCB then IC is getting damaged. I have observed some spark and fumes coming out from IC pins. 

Can you please help me out where I am doing wrong while testing the circuit.

-thanks

Regards,

Avinash