Hi, team.
My customer is considering power supply with the following specifications.
Input Voltage: 20 V
Output Voltage: 15 V
Output Current: ~ 0.5 A
Target: About $0.18
My customer don't want to attach external parts as as possible.
I am planning to promotion the LM317,Looking at the data sheet, there is a fear that there will be more external parts.
<Question>
When that consider a circuit that merely generates the voltage of the above specifications,is the minimum necessary external parts only the under parts?
· Input capacitor
· Output capacitor
· Two FB resistors
Best regards,
Masumi Sekiguchi