Hello,
i have a problem with a BQ78350 i try to run a learing cycle to update the FCC.
So i have too charge the battery near to full and then discharge to EDV2, right?
At the moment my FCC is set to 6144 mWh but it should something like 30700 mWh.
If i start charging it is stop by the Bq783350 at 6144 mWh cause the RSOC is 100% but the Battery isnt full.
How can i update my FCC?
best regards
Daniel