Hi, Dear
Datasheet said that if TPS54386 works in max duty cycle, and could not suport enough power for output, it will trigger UV comparator and goes into shut down and restart cycle. So does it shut down two channel output or only one channel with UV output? thanks.
This part is used in Car GPS power system, and it is powered by 14V battery, and has 8V and 3.3V outputs. when the battery voltage drops to near or below 8V, it will work in max duty cycle on 8V channel.
Thanks.