Team,
My customer has the following question regarding the TPS65218 powering up a AM335x processor.
I am troubleshooting another engineer's design
he has PWR_EN (pin 46) pulled up via a 100K resistor to the 3.3 volts generated by DCD4 (pin 15). the voltage input is 5V
I believe this is causing the PMIC device to occasionally not come out of reset (PGOOD is always low). I don't think this is good practice.
Ideally, I believe PWR_EN should be asserted high tbd msec after the input 5V has stabilized
and deasserted low tbd msec before or during when the main 5V goes out of regulation
during a shutdown
is this correct?
Regards,
Aaron