This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: What can cause the frequency higher than 2.2MHz

Part Number: LM5022
Other Parts Discussed in Thread: LM5122, LM5112

Hi!

I changed Rt to 20KOhm and from the equation, the LM5022 will posted to be about 830KHz operating frequency. But I measured the Vout and the waveform is about 11.1MHz, what can it cause the frequency higher than 2.2 MHz? Under this condition, the output is still stable for my set output voltage (2.5V).