This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63700: about IC loss

Part Number: TPS63700


Hi,

I am considering the following specifications.

specification
Input: 5 V
Output: -12 V
Current: 80 mA

Although I am considering the loss of the IC itself, I can not calculate it because there is no WEBENCH.
Can you tell how much loss of the IC itself? With the above specification.
Or is there a calculation tool?

Best Regards,