Hi,
My customers design uses an external resistor to set the output voltage.
Could you tell me the MIN and MAX values of Vfb?
If it is difficult to answer this question, would you please confirm the following?
The accuracy of the four output voltages is specified in the data sheet.
The MIN value is (0.8 V - 1.0%) V.
Since it is stated that external resistance accuracy is not included, the accuracy of VFB is also considered ± 1%.
Is this correct?
Thank you.