This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: I needed to design 1500W boost converter where output is 300VDC and input is 18VDC

Part Number: LM5022
Other Parts Discussed in Thread: LM5112, LM5122

Dear Sir,

So i wanted to design Boost converter of 1500W .,

Whose specification as follows ., 

Input DC supply:

1.) 16VDC-18VDC input 

Ouput DC supply:

Needed 300VDC-400VDC ( Current of 5A - 3.75A)

I designed using LM5022 , But got failed.,

Plz help me out..

Plz help me out..