Datasheet page-27 is described "total capacitance of 50 μH connected at PVCC node: 10-μF capacitor for buck converter of bq24133 and 40-μF capacitor for system side".
Is there calculation method for these capacitor value?
For example, below condition should increase capacitor value, is it correct?
・Io=2A, Vo=5V
・When AC/BAT switched (backup power) Δt=10us , Voltage drop (ΔV) should keep 0.1V
⇒Calculation: CxV = IxT
⇒ C = ΔIxΔT / ΔV
= 2 x 10u / 0.1 = 200uF
Best regards,
Satoshi