This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51362: minimum value of CSLEW

Guru 29720 points
Part Number: TPS51362

Hi Team,

My customer wants to ramp up VOUT(=1V) immediately after asserting EN high.
Is there minimum value of CSLEW for TPS51362? 
----------------------------------------

---------------------------------------

I believe there is no minimum CSLEW value as long as my customer takes acount of the following issue.
(datasheet page 17)
>The proper slew rate design minimizes large inductor current perturbation during the startup, thus reducing the possibility of acoustic noise in the system.

Is my understanding correct?

Best Regards,
Yaita / Japan disty