Hello,
I desgined TPS73733DCQR like before. But this time LAN8720A ic can not work well. The board have 4 layer. 1st layer is GND plane (all components is in 1st layer), 4th layer 3.3V power plane which is regulater with TPS73733.
TPS73733 have Enable pin which is enabling via MCU. MCU gets its power from another 3.3V LDO.
the problem LAN8720A can not work with these conditions.
1. if I give VIN 3.6V or higer voltage, Vout is 3.3V, it is ok but LAN8720 is Does not work.
2. If I connect EN pin to Vin, every thing is OK.
3. If I give VIN 3.5v or 3.3V every thing OK.
Board Current Consuption is about 175mA.
So what is Wrong??
TPS73733 is limitting the Current in 200mA?? or What is Wrong with enable pin??
Please help.