Other Parts Discussed in Thread: TPS61178
Hi,
We got a question from customer about TPS61089 and TPS61178.
Could you help us?
[Question]
They are considering to use the ICs under the following condition.
 Vin=2.7 to 7V
 Vout=4.5V
 Iout=2A
Their requirement is bypass operation(Vin=Vout) when input voltage exceed the set output voltage. They are thinking this IC can operate bypass operation.
Is their opinion right? If their opinion is right, how is the behavior of high side FET? To keep FET ON or turn-OFF(current through the body diode)?
Best Regards,
tateo