This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Searching for a LED Driver

I’m searching for a LED Driver with the following capability’s:

4 to 8 Channels output (depends on my designs)
Per channel 150 – 300mA output
Analog Dimming function for all channels (0- 5V?)
0 Volt on the Analog Dimming pin must switch all channels off

Overall input power is 12 to 24 Volt
The LEDs I use have an Orange color

On this moment I make use of the AL8805 and the Chinese PT4115 per channel. This costs a lot of space on my PCB’s with all the extra components.

So, I need one LED Driver what can do the all the above functions.

Thanks for your help,

Frank