Hi, we are using LM5576 Buck converter in one of our product.
Input for the LM5576 is from a battery bank around 60Vin and output is 12V , 0.3A output.
Switching frequency is 71KHz.
Now we face more nunmber of IC failure from the field at different conditions like sudden power on , either the input side of the IC got burnt and another type of failure is short at the output side across the switching Diode B/W pins 15,16 & 17,18. once we replace failure IC with new one some Boards are working fine, in some cases again the IC fails.
Herewith i attached the Design for reference also can you please propose a suitable LC filter and TVS configuration for our application.
Thanks in advance..