Hi
I have designed a Battery Pack with bq20z65 and 4 lithium ion cells in a 2p2 configuration.
Capacity estimation seems to be very correct at room temperature, RemCap gets a good value immediately after reset and tracks the situation very well during charge and discharge.
- After a full charge at room temperature does the EVSW show RemCap/FCC = 2400/2400 mAh (which is correct).
- I lower the temperature to -20 C, EVSW still shows RemCap/FCC= 2400/2400 mAh (The EVSW reads the temperature correctly ~-20C)
- I discharge with constant current = 1200 mA, during the first 75 minutes do RemCap decrease to 900 mAh but FCC is still 2400, when suddenly it jumps to RemCap/FCC = 0/1500, and the battery is empty.
It seems to me that only "coloumb counting" is used for continuos update of RemCap and FCC update after discharge, and no corrections are based on temperature or Impedance. (The circuit did measure the temperature, and the cell voltages mesured at 1200 mA, -20 C are significantly lower than at room temperature so the basis for a correct estimation seems to be there)
Do you have any idea of what I am doing wrong or have misunderstood?
Best Regards
/Mats