Other Parts Discussed in Thread: BQ25700
I want to use the BQ25700A in a new design but there are some things unclear, please help me with the following points:
- In the data sheet there are no thermal pad dimensions specified, could someone specify these?
- I want to use a 4.7uF Inductor, is this value allowed? And if so, what would be the IADPT resistor value?
- How should the ILIM_HIZ voltage divider resistor values be determined, and what is the function of this pin, only placing/releasing IC from HIZ mode or more?
- There is also an independent comparator with the CMPOUT and CMPIN pins but how could it be used and where could it be used for? there is very little information in the datasheet about this.
- Also looking at the parameters of the BQ25700 http://www.ti.com/product/BQ25700A/description, under special features is stated; "Solar Input" but the word solar is never used in the datasheet so what or where is this solar input?
Thanks,
Allard