Other Parts Discussed in Thread: TPS40170, LM5175, LM10011, LM5176
Hi,
I 'd like to create a new design most likely based upon the Lm25117-Q1 buck converter.
my requirements for the circuits are:
having 7 to 32V DC input voltage
output should be adjustable within the range of 3V to 30V DC were having around upto 4A @30V
is that realistically to achieve?
if not what's recommendable instead?
BR Oliver