Other Parts Discussed in Thread: TPS59640,
dear Sir
I saw TPS59640 can support VR12 ,But TPS59641 doesn't describe can support VR12
May I know TPS59641 support VR12 ??
What's the different between VR12 and TPS59641
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kai,
Looking at the product pages for both parts I'm only seeing IMVP7 compliance for both. Neither one states that it can support VR12 applications. You would have to look at the Intel specification documents to see if the devices would be compatible with VR12. The VID step size may not be supported (5mV vs 10mV or vice versa) as well as some accuracy specs on current monitoring. Also, there could be differences in performance between power states that may not make either part compatible with VR12.
For VR12 applications have you looked at the TPS53640 or TPS53631 controllers?
Thanks,
Carmen