This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355: Generating 1V from 12V input

Part Number: TPS53355
Other Parts Discussed in Thread: LM10011

Hi,

I am planning to use TPS53355 regulator for generating variable core smart reflex voltage for a keystone II device.

Core needs a current 28A max. 

Core voltage range: 0.8V to 1.1V

DAC used : LM10011.

Input voltage: 12V.

When I tried to open this regulator in WEBENCH, it gave the error: For these design inputs, the switching frequency of operation will be lower than the minimum supported by this device.

So please let me know whether i can use this device. If not, please suggest me any other device, best suited for my requirement.

Thanks in advance.

Regards,

Madhu.