Dear All,
one of my customer working on Dual USB charger based on TPS54260 device,
I have attached the schematics of dual charger for 48V input output 5v@2.5A.
Till now it is converting 48V to 5v at no load. When we put the load first voltage start decrease for 5.10V to 4.50v @0.6A .if we continuously increase the load at 0.8A the IC stop working ( showing input short ) . In the IC side VCC and GND showing short . kindly advise your valuable feedback.
Aravind.DUAL USB CHARGER.PDF