I have questions about TL594.
Question 1.
- In Application Report SPRA953C, 1.2 Test Card Impact(p.3), there are 1s and 2s2p about Rθja.
Is it 1s or 2s2p about TL594 Rθja?
Qurstion 2.
- In datasheet p.5 REFERENCE, Output-voltage change with temperature, maximum voltage is 10mV/V.
Are the following understandings correct?
Reference voltage is 5V. So, the voltage fluctuates by 50mv(=10mV/V x 5V) .
Question 3.
- In datasheet p.5, Frequency change with temperature, maximum frequency is 50Hz/kHz.
Are the following understandings correct?
For example, when frequency is 100kHz, the frequency fluctuates by 5kHz(=50Hz/kHz x 100kHz).
Question 4.
- TL594C and TL594I have different temperature ranges.
TL594C: 0~70°C
TL594I: -40~85°C
Is the fluctuate amount of TL594C and TL594I the same about Output-voltage change with temperature and Frequency change?
Best regards,
Takahiro Nishizawa