Other Parts Discussed in Thread: TPS40055
Dear, All
Customers are conducting evaluations using TPS40056.
Their circuits are made variable output voltage by externally inputting voltage to EA_REF.

When observing the waveform at startup, they observed the following problem when VOUT is 1.5V or less.
- HDRV pulse width is about 50ns
- There is no dead time when LDRV rise.
Waveforms of interest are not observed in normal waveforms. It occurs only at startup.

Although the charge current to the output capacitor was suspected, the same waveform is observed even if the capacitance of the output capacitor is made extremely small.
Please tell me the cause and measures.
Thanks, Masami M.