Other Parts Discussed in Thread: LMZ31704, LM10504, TPS25925, TPD1E05U06
when i use the LMZ10504,this module often damaged,the ouput pin has shorted to ground,
the input voltage is 4.5 and the output is 3V3.
please see the schematic and pcb figure.
on the power board,the 48V--5V power module output 5.5V to the blackplane,so there is a oring diode one he board,(the two power board will insert on the shelf)
then ,the5.5V from the blackplane is supply for LMZ10504
please help me,what had happend on the LMZ10504,thanks.