Part Number: LM5113
Other Parts Discussed in Thread: LMG1205
Hello,
Can you clarify that the two HS pins on the DSBGA device (namely pins C1 and D4) are internally connected on the die please?
It makes PCB routing a little easier to directly connect the C1 pin to the GaN FET gate return pin and only connect the D4 pin to the bootstrap capacitor (i.e. no need to physically wire C1 to D4 on the board).
Thank you,
Eamon