This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM53600-Q1: Vout_adj

Part Number: LM53600-Q1

Hi,

We got a question from customer about LM53600-Q1.
Could you help us?

[Question]
What is the condition of Vout_adj specified? They would like to know the value and the accuracy of feedback resistor.

Best Regards,
tateo

  • Hello Tateo-san,

    This datasheet parameter applies for output voltage range specified for adjustable devices which is 3.3 to 6V.

    The feedback resistors are usually chosen to be 1% tolerance, and nominal value for Rfbt = 100k. Bottom resistor in the divider can be calculated based on the equation (3) in the device datasheet.

    Best regards

    Brani