This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
requesting a circuit review for the UC3907.
When the output load current is 2.5A, when two SMPS are LOAD SHARE, each output current is measured as 1.35A, 1.15A.
How can reduce the two output current deviations?
Circuit configuration is as follows.