Hi
We have an application where we are regulating the input current to a non isolated 300W boost converter . The input voltage range is 3 to 60V . and the output voltage is 65V , We have an old design that is using a UC3535A PWM . We were trying to modify this recently to support a higher input current but we are seeing instability issues above with an input voltage from about 8V to 12V . Then we found that US3525A PWM does not support slope compensation and this could be the cause of our problem . The US3525A PWM as I understand it does not have support of slope compensation . Can you recommend a suitable replacement current mode PWM that supports slope compensation ?Are there any recommended replacements of the UC3525A PWM ? Can you also recommend any suitable reference designs or application notes .