Hi Team,
LM26484.docxPlease help with the below problem.
TI support is required as I in pre-production phase.
I have a problem with 3.3V supply on my boards:
(1) Burnt on 2 boards
(2) On working board we see ~0.5V ripple (182820.jpg file)
Observations:
(1) When reducing the input voltage from 5V to ~3.8V the ripple is significantly reduced (182804.jpg file)
(2) Other 1.8V, 1.35V and 1.0V voltages generated by the same DC-DC works ok.
(3) The output current is few hundreds mA.
(4) This is revision of board that worked ok at similar conditions (no changes in power supply section).
Attached relevant scheme section & relevant layout section.
Thanks,
Shlomi