This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65086: LDO3P3 & LDO5P0 Bypass

Part Number: TPS65086


For pins 54 LDO3P3 and pin 56 LDO5P0- If we are not using the outputs do we need to put the minimum value (2.2uF) capacitors for bypass? This is a space constrained application.

  • Hi Steve,

    The LDO3P3 and LDO5P0 are used internally for the part; the bypass capacitors are necessary to keep these stable and be able to provide any internal transient loads (though those will be quite small). It wasn't validated below the default values so I can't guarantee the performance of the part below the recommended values.