This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: 5 V Backwards when IC is off

Part Number: TPS54331

Hello,

we are currently using the IC above to convert 9V into 5V. To reduce safety precautions in production, we would like to power the circuit by an external connector.

Therefore the 5V is provided somewhere else, but will the IC get damaged if we supply 5V to PH/BOOT or VSENSE Pin ?

The schematic is confidential, but can be provided to engineers from TI.

Best regards,