This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: SMBus long clock stretching

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ78350

Hello,
customer uses the bq78350 with an ARM MCU. He recognise that the bq78350 SMBus has clock stretching >2ms and longer (after start 2ms to 8ms). The data are only requested every 100ms and the BMS is not charging or discharging. Is there a possiblilty to reduce the clock stretching timings?

Regards, Holger