Other Parts Discussed in Thread: TPS659037,
Hi all:
I have two questions about TPS659039 PMIC, as below:
1. Is there any formula about conversion die-temperature (adc result) to real Celsjus degree temperature??
I can read the gpadc channel 12 (die temperature) adc value, but i don't know how to transfer it to Celsjus degree temperature
how can i found it in the spec ?
I also found another formula, it can be used to TPS659037
( ( ADC_Read_Data / 2^12) * 1.25 ) – 0.753V
TEMP = --------------------------------------------------------
2.64mV
Is it can be used for TPS659039 ?
2. What is the difference between ch12 and ch13 in GPADC ??
I see the comment of them are the same, PMIC internal die temperature, so if i want to know pmic die temperature, read any of them is the same ??
Thanks!
Kenny