Part Number: TPS40170
Hello
I have a big problem to make DC converter to work.
Schematic:
Its based on Webench Designer project.
Main assumptions:
32-55V input voltage
5V @ 4-6A current
f=120kHz
Soft start 5-6ms (BTW. there must be a bug in Webench in calculating capacitor value for softstart, if I set any time, the result is always 2,2nF for SS Cap)
PCB Layout (2 layer):
Top:
Bottom:
After building prototype the first power up (40V Vin) was only 1,7V on the output.
I removed UVLO and bypassing it from Vdd (for testing at lower input voltage).
At about 8V to 13V i got a 5V on output but after incresing Vin at about 21V something happened (current limiter ?) and output drops to 1,7V. Now i cant get 5V at any Vin.
What i tested:
- different frequencies (100, 200, 300 kHz)
- longer soft start
- different Ilim resistor values
No way, it can't working.
Here some o'scopes:
2V/DIV in all screens
SS pin from 4,5 - 28V
SS pin (Vin 29V and more):
High side Gate pin:
Low side Gate pin:
Somebody can help with this magic ?