I'd like to configure the TPS65400 with following intialisation start up sequence.
Start-up sequence: - SW1(off _to_on -5V) >> SW2(off _to_on - (3V3) >> SW3(off _to_on -1V2).
Shut down sequnece SW3(on_to_off-1V2) >> SW2(on_to_off- 3V3) >> SW1(on_to_off- 5V)
SW4 (5V standby) = allways ON following power ON (Vin = 12V). Please confirm if this is an acceptable configuration.
Also, can I use SSx/PGx to control the sequence as the default. and overide EEPROM configuration.
SW1 = 5V standby (ENSW4 controlled by external logic) >>> PG4 to ENSW1. PG1 to ENSW2 and PG2 to ENSW3.