This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54526: Inductor value selection for TPS54526

Part Number: TPS54526

Hi,

I'm using TPS54526PWP in my design. 

I'm using it to generate 1.35V and 1.8V from 5V.

Please find the attached schematics for reference.

My question is whether I can use 2.2uH in place of 1.5uH inductor (output) as suggested in the datasheet ?

What will be the effects of 2.2uH instead of 1.5uH ?

Please let me know ASAP.