Other Parts Discussed in Thread: BQ78350, , BQ76930
Hi team,
My customer is using BQ78350+BQ76930+BQ76200 now, and meets one problem.
For 6 series Li battery with one BQ76200, the customer also uses a 16v TVS in parallel with the 100Mohm resistor.
For two battery package series application, they use the low side PACK+ connect with high side PACK-, and High side PACK+ as the +, the low side PACK- as the -.
For this condition, once short the circuit(pack+ connect pack-) and open one battery. The BQ76200 DSG cannot stand the -24v. It will make the device and mosfet fail.
From the datasheet, the min voltage is -0,3v, the DSG internal may have a 100V TVS.
Can we add one mosfet like BQ76930 below to solve the problem?
Thank you.