This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170-Q1: Circuit breaker

Genius 4840 points
Part Number: LM5170-Q1

Our customer consider to use LM5170-Q1.

Please advise us following their questions.

 

Question1

When NFAULT is High,is there case that circuit breaker doesn't work in this condition ?

 

Question2

Please send us equivalence circuit of BRKG pin and BRKS pin.

 

Regards,

  • Answer 1: The circuit breaker is powered by VIN. If UVLO is high, there are two different scenarios for the circuit breaker to turn on:
    (1) If the Fault Detection function is enable: VIN must be at least 10V higher than the 12V-port voltage.
    (2) If the Fault Detection is disabled by placing a 10k resistor across SYNCOUT and AGND: VIN must be at least a few volts higher (the breaker FETs' Vth).

    Answer 2: It is shown in the datasheet block diagram: a current source powered by VIN, sourcing current to BRKG, and a 12V internal Zener clamps the voltage across BRKG-BRKS, and an internal FET to pull down the BRKG to AGND to fast turn off the breaker FET.

    Thanks,
    Youhao Xi, System and Applications Engineering, APP-BMC-BCS, TI