This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS40210: Workbench simulation startup does not reach the requested output value

Part Number: TPS40210


Tool/software: WEBENCH® Design Tools

Hi,

I've just created the simulation in workbench to generate 95V @0.08mA from a 2C lipo (7.2-8.4Vin).

webench.ti.com/.../webench5.cgi

When I run the steady state simulation it works just fine and gives the desired output. But when I run the startup simulation it never reaches the output voltage. Is there a way to switch in the load after a certain time.

BEst regards,

Constantin