Part Number: TPS62740
Hi, I would like to use TPS62740 as a way to reduce the power consumption in a system comprising of a LiSocl2 battery one cc430 and one magnetometer. I'm not in electronics so much so I need some advice regarding the configuration of the system.
First, I need to decide if the magnetometer MMC5883MA (Datasheet) should be powered directly from the battery or from the TPS:
- The magnetomer is very low power itself (7 measurements/second -> 40 uA)
- As per application requirements, the magnetometer should detect approx 4 times a second in single detection mode
What's the best solution here? Is there any advantage if I power the magnetometer from the TPS? If I do, should I use the LOAD rail or the main rail? It seems to me that the LOAD rail activation would incur much more current consumption than the main rail and should be used only if I use a subsystem that can be disabled temporary so important power savings are obtain. On the other hand, if I power from the main rail wouldn't the normal activity of the radio and processor be affected by the magnetometer or the other way around?
Second, I can't see any usage in may case for the PG pin. If not used, what should be the value of the pull-up resistor?
Thanks,
Dragos