Other Parts Discussed in Thread: TPS62140A,
Tool/software: WEBENCH® Design Tools
Hi,
Webench used to design with 54228 as buck 2v to 5v with max current limit of 1.5A. While testing the circuit with load, the load reached (@5v+-) even more than 2.7A until it made the cut off. as it noted on the data sheet that it should limit the current cycle by cycle, please advice if 54228 can limit the current to 1.5A and is the webench back this design? and if so, which component we need to replace instead as in the attached webench simulation so we can get max 1.5A - meaning to stay there at max 1.5A even the load is higher?
Thanks