This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS714: Max Output current at 6.5V O/p

Part Number: TPS714
Other Parts Discussed in Thread: LM27761, LP5907

Can we use this LDO for the following application:

Voltage = +6.5V

Current limit power-up = 100mA

Steady State Current = 80mA

Ripple = 10mVRMS@1MHz

If not please suggest something else.